Megger

Megger

Megger - electrical testing from the utility to the socket

Megger is one of the world's leading premium manufacturers of T&M devices. We offer solutions to check the transmission paths of electrical energy from the power plant to the socket for their safety and functionality. There is a long list of Megger inventions such as Micro-ohmmeters, Insulation testers and DMM´s. Megger's famous hand cranked inductor has been synonymous with accurate insulation measurement for generations of electrical engineers. This was invented by our company founder Sidney Evershed in 1889.

Over the decades, we have continuously developed and expanded our product range in breadth and depth. Today, we can proudly claim to have played a leading role in T&M technology as the manufacturer with by far the longest tradition and the largest range. Our products combine many years of experience, the valued feedback from our global users with the inventiveness and conscientiousness of our product developers. Each subsequent series offers more safety and more reliability.

Featured products

The MFT-X1 - made with you in mind

Insulation testers up to 5 kV, 10 kV and 15 kV

The Meggers Advanced series with 5, 10 and 15 kV insulation testers is ideal for testing transformers, motors, switchgear and cables up to 230 kV. With support for IR, DAR, PI, DD, SV, ramp and PDC, it provides in-depth diagnostics for condition assessment and effective maintenance planning.

  • RE›Act test mode enables accurate measurements by monitoring absorption current.
  • PI Predictor™, memory and optional Bluetooth® enable rapid testing and easy data export without manual recording.
  • Free documentation management with CertSuite for simple and efficient documentation.
The MPAC208 is a professional acoustic imaging camera

MPAC208 – acoustic camera

The MPAC208 is a professional acoustic imaging camera designed for rapid and precise detection of ultrasound sources in industrial environments. It helps maintenance teams identify gas leaks, mechanical deterioration and partial discharges (PD) in high-voltage systems, without the need to interrupt operations.

  • 208-channel MEMS microphone (2–100 kHz) enables detection of very small leaks and subtle ultrasound patterns.
  • Acoustic data is combined with a 13 MP camera and 8" touchscreen that displays sound sources directly in real time.
  • The MPAC208-IECEx has the same features as the standard model and is certified for Class 2 hazardous explosive atmospheres.
Megger utility products

Protect your assets for a reliable, sustainable future

In today’s evolving energy landscape, maintaining critical infrastructure is key. Megger’s advanced testing solutions ensure reliability, reduce downtime, and prevent costly failures, helping utilities and energy providers protect vital assets.

  • Insulation Testing: Detect degradation early for safety and efficiency.
  • Acoustic Imaging: Pinpoint partial discharges to extend equipment life.
  • Low Resistance Testing: Ensure stable connections for a reliable network.
The MFT-X1 is a powerful multifunction instrument for demanding electrical professionals

The all-round solution for professional electrical testing

The MFT-X1 is a powerful multifunction instrument for demanding electrical professionals. With the highest precision, efficient handling and versatility, it reliably supports installation testing, verification of protective measures as well as earthing and EV tests.

View now

Continuity & low resistance testing

The purpose of an electrical continuity test is to establish just that; the circuit is continuous.

Is it used by electricians to be certain that no wires have been crossed at a junction box and all connections are correct and tight.

Hundreds of similar applications assure that electrical continuity has been established or maintained. Similarly, diodes and other components are readily tested. Often, an actual measurement isn’t needed; the IUT passes by a pre-set buzzer.

TDR family

The greatest experience in runtime and cable length measurement

The method is also known as TDR (Time Domain Reflectometry), which describes the analysis of cable length and reflection characteristics of electro-magnetic signals and waves in electrical conductors. Some people know this technology also under the name "cable radar” as the principle is indeed similar to a conventional radar.

The length measurement of cables in the electrical industry was one of the first important applications. electrical industry was one of the first important applications.

Earth testing

Megger ground testers offer unique solutions for your grounding measurements. As well as complete sets of measuring instruments, measuring leads and stakes in a robust hard case - and thus everything that is needed for measurements on site. The housings of our earthing measuring devices usually offer protection class IP54 and are therefore suitable for outdoor use.

All our measuring instruments are designed to be user-friendly our earthing measuring devices usually offer protection class IP54 and are therefore suitable for outdoor use. All our measuring instruments are designed to be user-friendly